In our current hardware platform FPGA is connected with WL1835MOD using SDIO interface instead of CPU. But when I looked into WL1835MOD's datasheet and other document I can find nothing about how to operate WL1835MOD, it just said that WL1835MOD should connect to host processor using SDIO. So what should I do to drive WL1835MOD directly without software working? Or is there any document descriping details about how to operate WL1835?
BTW: I found on datasheet there are two pins named GPIO1 and GPIO2. And the description of these pins are WL_RS232_TX and WL_RS232_RX? Does that mean I can drive WL_RS232_TX pin with what I want to transmit instead of using SDIO interface?