In the TI literature, I see numerous block diagrams of a system with a HUB transmitting 4 independent audio channels to 4 independent RECEIVERS.
I don't want to purchase a bunch of eval kits, only to then discover that what I am trying to accomplish is not possible. So, I have a number of questions first ...
- Is it possible to do this to reverse? So, having four independent SOURCES transmitted back to a single HUB, yielding 4 independent audio output channels at the output of the HUB for mixing/recording?
- I think this may be where the SOURCES (protocol slaves) would be set to 12-15?
- If that is correct, what would the HUB (protocol master) be set to?
- I assume each node (SOURCES and HUB) would need to be a CC8530?
- What configurations should be used in the SOURCES/HUB in the TI Configurator Software?
- If there is not a standard configuration, is it possible to develop one? At a high level, could you describe what we will need to accomplish?
- Regarding your suggestions for above, would there be any difference when just a single SOURCE is used (or, 2, and 3 SOURCES) instead of all four SOURCES? For instance, should the system know how many SOURCES are connected to the network, and use Dynamic Audio Channel Selection in those situations?
- Can this be prototyped using the Eval Kits. What would be required (four CC85XXDK?)?
Thank you!