Will there be a firmware update that allows the use of the recently released CC2592 range extender? Would I need new firmware to use the chip? Is there any reason to use the CC2590/1 over the CC2592?
Thanks,
Pedro
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Pedro,
From a configurator/firmware perspective there is no difference between the CC2591 and CC2592. Use the CC2591.
Due to ETSI regulations, you can not exceed what can be output from CC85xx+CC2590 in Europe. Using the CC2592 and then backing down the output power will be energy inefficient vs. the CC2590, but there might be a small improvement in sensitivity with the CC2592 combinations (and also slightly easier to design with) so in the end it is up to you.
There might also be price differences between these devices. Please contact your TI account or distribution for this.
Kjetil