Hello,
We have developped a wireless phone unit using ce CC8530 and it works fine. (monophonic full duplex)
We have also made on the same idea a headset unit using the CC8530 (stereo M>S and mono S>M)
We need to use about 12 units like that in the same room. As each unit use 4 channels at 20% among the 18 existing channels. This configuration seems to use about 50% of the complete allowed frequency band.
Have you any informations or recommendations for the use of some wifi channels in the same place?
Il i want to use more headsets, does the slac compression helps for reducing the channel occupation?
As the SLAC gives about 1/3 of bit rate does that means we can have three time more users in the same room?
Thank you for your help
Bernard