I have an application in which I'd like 16 slave units to connect and stream audio to 4 masters. They must do this in an environment where there's likely to be a fair bit of WiFi interference (auditorium). Similar posts in this forum lead me to believe that 3-5 masters is possible, but not in a noisy environment. Here are my questions:
1. Can I dynamically define what frequency constitutes a channel? If there's enough room in the 2.4 GHz band, I should be able to offset those frequencies so each master operates in its own 18-channel space without risk of interference from the other masters.
2. Can I dynamically alter the hop sequence?
3. If I can dynamically define the hop frequencies and sequence, I will need to tweak the pairing algorithm to ensure a slave gets an appropriate assignment on a well-defined channel (similar to a "listening socket" in TCP/IP). Do I have the ability to tweak the firmware to make this happen, or can I make this happen simply micromanaging the device through a host controller?
Finally, I would like to take the I2S stream from each master and do some mixing and light signal processing. Does TI have a recommendation for a Swiss army chip, or am I better off mixing separately and allocating a single DSP to each 8531?
Regards,
Mike