Hi
I am setting up a static home multi-room system. I have 2 headset kits, configured as 1 master and 3 slaves.
They work OK, but I want to leave them 'always on', powered from mains-USB chargers. I am happy to leave the supplied batteries connected. I have set the Power control on master and slaves to 'None', but after a while (overnight, coming back from work) I still seem to need to unplug the USB charger from the board, and/or turn the units on, and/or pair them .
I have seen
http://e2e.ti.com/support/wireless_connectivity/f/382/p/205553/729558.aspx#729558
but as I read it, the 6 hour power down should not happen if there is a battery connected.
Do you have any other suggestions ?
Also, is there any way to reduce the intensity of the 'battery charging' LED - it is so bright it is hard to see what the Status LED is telling me.
Thank you
John Robinson