Hi,
We have been using the CC85XX-CC2590EM reference design in our products for a quite a while now. Our RF boards are exact copies of the reference design.
We have been using two different subcontractors for the manufacturing of these boards, let us call them subcontractor A and B. It turns out that the RF performance of the inverted F antenna when using boards from A are way better than when using boards from B. The differences are quite extreme, even though both subcontractors have been given the exact same gerber files and specifications. When using master and slave boards from B, drop-outs are constantly occuring, and the system is useless. When using master and slave boards from A, no drop-outs occur at all, even when trying to provoke it by all possible means.
I am now trying to figure out how this is possible, and how to avoid it. My current suspicion is that the two manufacturers are not using the same dielectrics and/or not interpreting the manufacturing specification the same way.
Question 1:
Is the outer layer copper thickness crucial for optimum RF performance?
Question 2:
As stated in the CC85XX-CC2590EM readme file, the outer layer copper thickness should be 35 um. Is this the non-finished copper thickness or the end thickness after plating?
Question 3:
Outer layer plating is not specified. What is the optimal type and thickness of the plating?
Question 4:
Can an inadequate choice of dielectrics type and/or thickness cause the effects described above?
Best regards,
Torje