Hello,
I am at the end of my long development project and I have come across a very unpleasant surprise - I cannot configure a master for 4 slaves at PCM16 quality with 2 channels - the software allows this configuration but at the flashing it says robustness below the criticality level. The most it allows to choose is 3.
One thing this is very misleading and unfriendly way of presenting limitations - in most cases the GUI simply does not allow to choose unsupported combinations.
But more importantly it is in clear contradiction with the clear statement on p. 45 of the Family USer Guide:
"Note the following guidelines/limitations when selecting streaming formats: 1 or 2 channels: No restrictions" - SWRU250L
In my view using up to 3 slaves instead of specified maximum allowable 4 is a clear "restriction" ?
How I can make this configutration work ? - ability to stream stereo PCM16 to 4 slaves is the key technical and functional assumption for my business project and significant investment.
I would appreciate an answer possibly soon.
Regards, Pawel