Hi,
we want to design a wireless 7.1 and 5.1 sound system. The base station consists of two CC8530 synchronized by timeslot alignment. The base station should be connected to a PC running Windows or Linux and for this reason we need a USB interface to the two CC8530. Unfortunately the CC8530 don't have a USB interface. What would be a simple solution to add a USB sound card feature (like CC8531) to the base station?
Thank you for your support!