With the CC85xx Development Kit's Preloaded Demo, the PurePath Wireless Configurator shows the Range Extender is set to "CC2590 (HGM)" for both the master (Tx) and slave (Rx). Does this "CC2590 (HGM)" setting insure that the max 14 dBm output power available on the CC2590 chip is being used? I measured the transmit output power of this Dev Kit with a VNA right at the SMA antenna connector and got around 11 dBm. How can I get this transmit power up to the 14 dBM max with the PurePath Wireless Configurator?