HI All,
i have an application with 4x mono microphones to from the one consumer. Can I, from the consume,r remotely disconnect a microphone (CC8520) from the network and place it in a low power state. Thus can I then ask the producer to rejoin the network remotely?
My devices are all host controlled and i will be using the side data channel. If however I remove one microphone from the network i can invoke it to rejoin using my host processor but I would like this facility at the consumer end. I want to do this to save power as all mics are running on batteries. Think four independent presenters with a wireless mic each. I want to remotely switch them on at will.
Ideally the microphones would go into a low power rx-only mode.
Thank you all in advance,
James