Hello,
I have managed to get both the HostTestRelease (via USB) and the SimpleBLEPeripheral compliling, working, and communicating between the two devices using BTool no problem. What I'd like to do now is redirect the HCI communication (on HostTestRelease side) with BTool, from USB to serial (UART0). It looks like in the build if I associate CC2540EB directory with the build instead of the default CC2540USB, it should use the UART instead of USB for HCI coms to BTool - is this correct?
If not what is the best solution and suggested way forward?
If I and correct, then am I missing a define somewhere? Any information would be a help.
Also if it is possible to use HCI over UART;
Where is the baud rate set, parity, stop bits etc (defaults?),
Should the code for HCI-over-serial use the DMA option or ISR (which one is it built for)?
BYW, the reason for wanting HCI over serial (UART) is our next stage in embedding the CC2540 into a non-USB platform; and spying BTool when necessary would be an advantage.
Thanks in advance,
Edward