Hi everyone! I need to measure my connection interval which was set in 100 ms.
But i need to do some tests and i don´t sure that the connection interval was set correctly.
I proved with an oscilloscope the SimpleBlePeripheral disabling
all periodic and external events.
In Osal.c:
osal_run_system( void ){
...
osal_pwrmgr_powerconserve();
P1_7 ^= 1;
}
So for only in a connection interval the proccessor should wake up.
But when i measure the P1_7 pin shows a signal of 500ms instead of 100ms.
Any help will be appreciated.
Thanks, Greetings to all!
Martin Romero