Hi,
I'm using the "Simple Peripheral Profile" project of CC2541 (mini development kit).
Is there a way of enabling notification for specific characteristic within the server as opposed to by command from the client (BTool)?
Is there a way for the application in the server to know when the client enables/disables notification for specific characteristic?
I also don't understand the following:
does this what enables the notification for Characteristic ?
// Characteristic 4 configuration
{
{ ATT_BT_UUID_SIZE, clientCharCfgUUID },
GATT_PERMIT_READ | GATT_PERMIT_WRITE,
0,
(uint8 *)simpleProfileChar4Config
},
if so how different will it be if I want to enable it in Characteristic 5?, how should I declare simpleProfileChar5Config, I understand from the spec that clientCharCfgUUID will be used for every Characteristic, how can I find the right handle no to have the client write the notification enable to?
Regards Igal