I have running the CC2541 and the tps62730 successfully.
Now I want to add the CC2590 for extended operating range. Is it still possible to use the tps62730 in a design
together with the CC2590 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The TPS62730 has a maximum current rating og 100 mA so it can be used to power the CC2590. Note that the output power of the CC2590 is supply voltage dependent so by using the regulator you also limit maximum output power.
Cheers,
Fredrik