Hi
I just want to find out if I am using the right profiles.
Device A (SmartPhone) is the Broadcaster and Device B is the Observer.
1. Device A will send out an advertisement. Device B will read the advertisement and then turn into a Broadcaster to send the desired sensor information. So I assume Device A will then need to become an Observer to read the sensor info.
2. Will it be possible to send information from Device A Broadcaster to the Observer to change the Device B GAP_ADTYPE_LOCAL_NAME for example from SensorTag1 to SensorTag5. I would like the Smartphone to only target the Sensortag number of my choosing.
3. Is OAD possible in all profiles or do you have to pair to do an Over the air download?
Thanks.