Hi,
How can I alter attributes of the Accelerometer and the Gyro included in your BLE cc2541 Sensor Tag board by using the Iphone and the Android smartphones following download of the application software.
For the cc2541 SensorTag, Using the Smartphone, how do I set the Cutoff frequency of the Accelerometer to 5 Hz and
its sensitivity to 2 G; also how do I set the sensitivity of the Gyro to 1000 degrees per sec. and its cutoff frequency to 10 Hz?
Is it possible?
Thanks.