hello, i just got a cc2541 sensor kit, after a first try at the android app (where i had readings) i connected it to an ipad, the device told me that it needed an updated firmware. connection was lost during upload so now my sensor tag has no firmware.
i reuploaded image A from my android phone, but it still tells me in the upload window that the current image is "Not an OAD image"
did i brick my sensor day one ? or can i reset is somehow ?
after uploading A again, i can now see the device on android with only buttons, and it does not work. if i change sensors option i got a "gatt error 3" message on overlay
on ipad it say 'no profile or sensors enabled click settings to configure device' but there is no such options