Hi,
We have done significant developing of a project using the HIDAdvRemote as framework. We now see the need to increase the transmit power of the remote to 4dB from the default power of 0dB. This is not possible with the cc2541 chip which the HIDAdvRemote is built for. Therefore we are asking if anyone has a project which has modified the HIDAdvRemote to work with cc2540, or if TI has this project available, perhaps in a latest release or beta version. The stack we are using is the BLE-CC254x-1.3.2.
Thank you