Hi everyone:
Cc debugger after finished burning bootload, insert the usb computer, started burning "cebal fw srf05dbg.hex", appear "cc debugger firmware verification failed" error, is chip problem excuse me? Or where the configuration problem?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi everyone:
Cc debugger after finished burning bootload, insert the usb computer, started burning "cebal fw srf05dbg.hex", appear "cc debugger firmware verification failed" error, is chip problem excuse me? Or where the configuration problem?
Hi,
I want to make sure I understand your situation correctly. Is this how it happened?
- You plugged the CC Debugger into the computer
- You opened SmartRF Flash Programmer
- You were prompted to update the firmware of the CC Debugger
- During the update process, SmartRF Flash Programmer reported that verification failed
Is the CC Debugger still functional? Do you happen to have another CC Debugger? You can probably use one to re-flash the other if bootloading has failed.
Peder
HI:
I am in own homemade CC the DEBUG, I now use CC2511 production batch number is 1401, I've used in the production of CC debugger CC2511 production batches of 1319, The 1319 don't have any problem, is the no. 1401 in other writing bootload downloader to burn is no problem, just the usb connection to a computer this problem!
Hi,
Did you copy the schematic of the CC Debugger exactly? Flash verification failure can mean that there's an issue with the power.
We changed the package of CC2511 last year. There is no functional difference between the versions.
Peder