After Loading the Firmware of CC2451 Keyfob over the Air Via CC debugger using SmartRF flash Programming.
I Can not Scan the CC2541 keyfob any more .Please suggest the solution.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can't understand question clearly.
Do you mean , you updated image via OAD or via programmer?
For OAD choose "CC2541DK-Sensor-OAD_ImgA"configurations while building the image and when you want to flash image using "Erase, program and verify" option choose "CC2541DK -Sensor" setting for building hex file.
Hi
I have loaded the firmware i.r .Hex file using SmartRF Flash Programmer and after doing this i can not Scan/detect the BLE device.
Thanks a lot for your coordination.
Hi,
Which configurations have you chosen while building hex file.
On left top IAR embedded workbench, which workspace configurations have you chosen?
Can you describe steps which you have done? It'll be more helpful to understand problem.
thank you.
Hi
Below are the step i have followed .
To read or write a hex file to the CC2540/41, select the “System-on-Chip” tab (default). The connected
CC2540/41 should be detected and show up in the list of devices. Under “Flash image” select the desired
hex file that you would like to write to the device. If you are reading from the CC2540/41, under “Flash
image” enter the desired path and filename for the hex file. To write to the CC2540/41, under “Actions”
select “Erase, program and verify”. To read from the CC2540/41, under “Actions” select “Read flash into
hex-file”. To begin the read or write, click the button “Perform actions”.
After this i can not scan /detect the device .
IS there any way i can reset the BLE device?
Thank You