Hi,
There is a doubt which need to be clarified
In the structure attHandleValueNoti_t structure in att.h file
typedef struct
{
uint16 handle;
uint8 len;
uint8 value[ATT_MTU_SIZE -3];
}attHandleValueNoti_t;
The field uint8 value[ATT_MTU_SIZE - 3] can it be change to uint8 value[150];
If changed what will happen ? Is there any problems associated if changed ?
Regards,
Rakesh