Hey guys,
I am trying to create a new profile on KeyFobDemo. I was able to modify Characteristic 5 on the SimplePeripheral example to read and write 22 bytes. However, when I try to use the same structure on my KeyFobDemo profile I cannot write/read more than 7 bytes...
I am using the osal_memcpy technique i have seen in other discussions. My guess is that the osal_mem is out of space which is causing the error? If anyone has an idea of what the problem could be that would be greatly appreciated.
In addition, I eventually need to store this data in flash (not using z-stack) and read multiple packets (incoming data from phone will be around 6KB. Therefore any advice, examples, or resources on how to implement that would be great. I haven't found any useful forums on this topic.
Requesting a response as soon as possible.
Thanks,
Adam