Hi
I need to make ONE costum profile with following UUID's:
GATT service with UUID: E20A39F4-73F5-4BC4-A12F-17D1AD07A961
Device characteristic with UUID: 08590F7E-DB05-467E-8757-72F6FAEB13D4
Data characteristic with UUID: 08590F7E-DB05-467E-8757-72F6FAEB13D2
I use SimpleBLEPeripheal project as template but i cannot find where to type in the "new" UUID
One place where i have found UUID (128Bit) is here:
// TI Base 128-bit UUID: F000XXXX-0451-4000-B000-000000000000
#define TI_BASE_UUID_128( uuid ) 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0xB0, \
0x00, 0x40, 0x51, 0x04, LO_UINT16( uuid ), HI_UINT16( uuid ), 0x00, 0xF0
When i chage it here the BLE Device Monitor tool do not show any different values !!!
Can someone tell me how this costum profile corresponds to the GATT service 00:18 (Generic Access Profile)
01:18 (Generic Attribute Service) and for example 0A:18 (Device Information Service)
Are above GATT services still available after a new profile has been implemented or is the GATT services replaced ?
Hope for a quick reply, thanks in advance.
Kind regards
Christian