Hello,
Can I store and access the memory in CC2541. I want to store few sets of data. such as numbers in CC2541 and be able to access it later in time. Is this possible?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
If you are asking whether you'll be able to access it even after cc2541 is turned off...
You can store data in Non Volatile memory of CC2541. You can use osal_snv_write and read functions Which are located at "C:\Texas Instruments\BLE_CC254x_140\Components\osal\mcu\cc2540\osal_snv.c".
You can store data upto 64 KB. For storing data you need to use IDs which indicates flash page area.
For example,
Format: uint8 osal_snv_write( osalSnvId_t id, osalSnvLen_t len, void *pBuf )
id can be from 80-FF.
len is length of data and pbuf is buffer of data.
-------------------------------------------------------------
Press "Verify" if your question is answered.