I want to use the CC2541 as data streamer.
I want to write a program for sampling some sensors and send the data over the air
I also have to get command from the master unit , and response with status notifications.
I look at the BLE bridge APP and it look good to use.
I just need to change the data receive/transmit from/to the UART to internal buffer.
For assessment the "room" I need for the code I compile that APP in DMA mode and get about 117K byte code.
It is look to big for this App.
1. Is this App good for my need or I can get better App that do the some with less code area?
2. Does those figures are close to reality?
3. How much code I will be save if I don't use the UART capability?
4. Does the CC2541 has a good OTA APP, and where I can find it?
Thanks
Bar.