Hi,
I have a CC2540EMK-USB which is pre-programmed to operate as packet sniffer.
I also have a CC2541 Sensor Tag. I want to connect the CC2540EMK-USB and CC2541. What steps do I need?
In the quick start guide, there is mention of using the SensorTag with BLE Device monitor. BLE device monitor does not work "No response from BLE host".
Do I need to upload the correct image to the CC2540 dongle CC2540_USBdongle_HostTestRelease_All.hex?
If so, will the packet sniffer functionality still work with this image?
Regards,
Andy