Hello,
I'm using CC2541 to communicate between my cell phone and external microcontroller . However, I also want to use and program the inbuilt microcontroller of CC2541 and make use of its digital I/O pins. Can CC2541 continue communicating fine with the phone when I have connected it to external microcontroller and also using it's inbuilt microcontroller?
My concern is that would mess up the I2C communication since CC2541 would be acting as slave device for Bluetooth communication while the microcontroller inside it would be acting as a master to this slave device.
Also, if this is possible, can I use just the smartRF Flash Programmer to program it or do I need anything else as well.
Thanks!