Battery of the board based on CC2541 is consumed so fast. Please let me know how to improve this or if additional schematic is needed.
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Battery of the board based on CC2541 is consumed so fast. Please let me know how to improve this or if additional schematic is needed.
Thank you.
Hi,
The on-board peripherals should be in deep sleep/disabled/hibernate when not in use. Also the GPIOs should be configured properly when not in use. This will help you to reduce the power consumption while device not in use.
Also you may consider to reduce the Transmission power by changing the TXPOWER register and also set the same value in advertising data. It will help you to reduce the power consumption while device is active. The transmission of data takes maximum power, so send data less frequently if possible.
You can refer this application note.
Hope this helps.
=====================================================================================
If this has answered your question, you may consider to "Verify Answer".