Hi Everyone,
I doing a project where i will be powering my BLE module for a very short time. i am looking for ways to cut my current consumption and on time.
1. I know that the slave has to advertise before a connection can be made. But what about if the master knows the slaves address and wants to make a direct connection without the slave advertising. is that possible?
2. I am using the Blueradios module and with that you can stream data when the master and slave are connected. Also i am sending packets from my custom made application through the uart for the slave to send me a packet. I noticed that a when i increased the connection event time, even though i keep on sending packets , they are not received at the slave end for a while(10-15sec), even though the maximum connection interval is 4sec. Any help??
3. Does anyone have an idea if bluetooth is suited for such an application. The slave will be powered for a maximum of 300msec.?