I am testing some code on the SensorTag and I have noticed that in the part list and the schematics it is noted that the accelerometer is KIONIX KXTJ9-1007, but when I look at the code supplied with the CC2541EVM I can see that the register addresses match a different accelerometer - KXTF9-4100.
Is the mistake in the schematics or the code.
I would like to use the example and add my own code – will the accelerometer work?
1234.cc2541 Presentation1.pptx