I have Keyfob –CC2541DK-Mini Development kit
1. need to add few more events at the CC2541 keyfob unit to the present keyfob working code and the same has to be activated from the master unit (CC2540 USB- connected to PC)
(similar to accelerometer – enable /disable from the master and receive the data via master if enabled at the keyfob unit)
Q: which section of the code we can modify
2. At the USB side we would like to add few more Characteristic value handle and Value apart from what is available as default –
Q: which section of the code we can modify
3. At the BLE-CC254x-1.4.0 software bundle for IAR environment we find the CC2541 and CC2540 with common source files.
\\BLE-CC254x-1.4.0\Projects\ble\KeyFob\CC2541DB\ KeyFobDemo.eww
\ \BLE-CC254x-1.4.0\Projects\ble\KeyFob\CC2540DB\ KeyFobDemo.eww
\ \BLE-CC254x-1.4.0\Projects\ble\KeyFob\Source
Q:
a. Hope the \ \BLE-CC254x-1.4.0\Projects\ble\KeyFob\CC2540DB\ KeyFobDemo.eww is used for the USB dongle unit (CC2540)
b. Hope we can not have the same work directory to modify both the keyfob unit (CC2540) and USB unit(CC2540) source code and needs to be a separate working director for each due to common C source files.
Thanks for the reply