I have been reading various posts that state that using notifications (when using a CC254x) will increase the amount of data that can be transferred from a peripheral server to a client.
Various examples have been given: Some use GATT_Notification while others use GATTServApp_ProcessCharCfg to invoke the notification. It appears that GATT_Notification is more direct, while GATTServApp_ProcessCharCfg is intended to be used in the "SetParameter" function.
It sounds like folks have gotten both methods to work. Which is the preferred way? Which yields better performance? Will both methods permit multiple notifications to be transmitted in a single connection interval?
Most examples that use GATT_Notification show the use of a "dummy" handle. Is this just for the example? Shouldn't this point back to the characteristic attribute?
IAny enlightenment would be appreciated!
Thanks!