As I understand the only difference between CC2540 and CC2541 is USB on the former and I2C on the later. I want to use SensorTag fw and iOS app, but SensorTag mostly refered to CC2541.
I was mostly working with CC2540, I wonder if I can use the existing CC2540 PCB that I have to start using SensorTag as a starting point?