hi,
I want to interface SPI memory chip-AT45DB021E (www.adestotech.com/.../doc8789.pdf) with cc2541 for extra storage purpose.
configuration is as shown below:-
memory side cc2541 side
SI - P1_5
SO - P1_4
SCK - P1_3
CS_N - P1_2
I already interface (UART) msp430 with cc2541 by simply adding serialInterface.c/h file to simpleBLEBroadcaster code (because i also want advertising on cc2541) as suggested in link:-processors.wiki.ti.com/.../SimpleBLEPeripheral_SerialInterface.
msp430 side cc2541 Side
P3.4 (TX) P0_7 (RX)
P3.5 (RX) P0_6 (TX)
in UART code where should i define these pin configaration?
can you give me hint on spi memory chip interfacing (SPI interfacing).
Thank u in advance.