Hello CC Team,
Excellent product. Just waiting to get my hands on one.
Looking at the schematic for the DevPack, I can't see the TM4C1294NC being just a randomly selected Chip. Please tell me that pins 53,54 and 56,57 lead to one of the unpopulated connector spots and are not terminated under the chip. I hope the designer had an Edge Router in mind when they made the arguement for selecting that particular chip.
Access to all the other pins, especially the QEI and PWM would make the DevPack an undisputed must have for any developer. Please say it is so.
Also, it doesn't clearly state that:
1. The SensorTag can be programmed with an existing SmartRF06
2. Or if the free CCS 6 license applies only to the DevPack purchase or the CCS 6 license is free when used with a SensorTag.
Thanks,