Hey Guys,
My name is Birkan and Im working on Android project to connect over bluetooth 4.0 via beaglebone black. I build my own android version and kernel and it boots but Im facing some problem, before I build I configured Beaglebone board and they are attached on this post. and Im using this ble module on the picture which has TI CC2541. and My connection is
From BLE module TO Beaglebone black
RX >>>>>>>>>>>>>>>>> TX (Uart1 P9_24)
TX >>>>>>>>>>>>>>>>> RX (Uart1 P9_26)
5V >>>>>>>>>>>>>>>> 5V (P9_6)
GND >>>>>>>>>>>>>> GND (P9_2)
After boot, I go settings and click bluetooth settings. I see black page without any buttons just only back button down. I dont understand the problem. Maybe Im connection to wrong pins or Im using wrong interface.
Im totally open for any suggestion and try. Im working on it for more than 2 weeks. I need your helps guys.
Best Regards
Birkan
Birkanconf.zip