I have a couple questions regarding the new SensorTags:
1. On the CC2650STK webpage, it states "The new SensorTag is based on the CC2650 wireless MCU, offering 75% lower power consumption than previous Bluetooth Smart products." Is this in comparison to the CC2451 SensorTag? If so, how was this power consumption measured?
2. Is the firmware from the CC2541 SensorTag easily ported to the new CC2650 SensorTag platform? What would need to be adjusted to make sure that prior software designs can be supported on this new SensorTag?