CCS is returning error 'unable to connect to target' when i try to run and debug the SensorTag with the DevPack (see details below).
Any ideas as to what might be the problem?
Thanks, Zaffer
CCS error details:
Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during
the connect returned bad status or an error.
The cause may be one or more of: invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
(Emulation package 5.1.641.0)