I reading now the timer APIfrom HAL Drivers API SWRA193 Version 1.6 and there some missing documentation . Also the is no source code in BLE-STACK 1.4.1 for the timer part.
1. I found on the forum the hal_timerץב ודק כםר CC253X but it is not full support of the CC254x especialy multi channels and compare modes. Is there a new and full version of this code avalible?
2. I don't see how the configuration take effect it the HAL , because TimerInit only put default values and not the ones set it the config phase?
3. There is no description for the prescale settin gin the API doc. Also where it take place after the init or before?
4. When I use the timer as compare I don't see where the compare value place in the param.
5. If i don't use the interrupt and want to use the HalTimerTick (void) function. Does it active automaticly or I need to make soem settin gto make it call every tick?
Thanks
Bar.