Can I use an external debugger (a Segger JLINK ARM in fact) with the SmartRF06 to debug a CC2650 board? I know I can go the other way and use the onboard XDS100 to debug an external board, but I want to plug an external Segger into the cortex ARM 10-pin header and use that instead of the XDS100. Reason, XDS is windows and linux, I'm on OSX, I have a JLink ARM which works on OSX, I believe it supports the CC2650, so I was going to try that out.
If so - what jumpers do I have to pull? I assume I disconnect the jumpers from the XDS bypass header, but will that still leave the debug header connected to the CC2560 daughter board or disconnect it? I can't find a circuit diagram for the SmartRF06 so I can't tell which side of the whole thing the bypass header is.