I just received a SensorTag Development Kit Featuring the CC2650 wireless MCU and it's completely dead after 1 day of light use.
Hopefully is the battery. Is there a chance that the CR2032 lithium battery might run out in just a day?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I just received a SensorTag Development Kit Featuring the CC2650 wireless MCU and it's completely dead after 1 day of light use.
Hopefully is the battery. Is there a chance that the CR2032 lithium battery might run out in just a day?
Thanks.
I purchased two sensortags(CC2650x) a few weeks ago. The one I have been using heavily is still running. The other one which I used just a couple of times is dead, battery is dead. AFAIK it was doing nothing.
Is it possible that the batteries shipped with the units are of lesser quality...like the first battery you get with a car or a remote control?
If you have any rough estimates on battery life in low, medium, high usage scenarios it would be helpful.
Thanks.
I have the same issue (CC2650, fw 1.01, hw PCB 1.2).
I have used the battery that came with the sensor, and a new one. Currently using my 3rd battery.
For both:
So, not quite the advertised "years of battery lifetime from a single coin cell battery".
Any suggestions?
Update: and the same for the 3rd battery: empty after a few hours (and switched on for less than 5 minutes). It has only been connected to the standard iOS TI Sensortag app.
Any update on battery life? I'm no my 3rd battery. only played with TI Sensortag app and attempted to connect otherwise to an app I'm writing.
Cristin,
(I apologize for posting and then not being able to follow up. I've been out of town without the sensortag.)
The information on the back label is
1 6 4 2
BLE
Rev. 1.3.2
F W Rev. 1.2.1
The hardware rev is 1.2/1.3 (1.3 on the PCB silkscreen).
Firmware revision is 1.30 (May 23 2016).
Leonard
The SensorTag V4.0.6 app enables all the sensors initially.
I have run it at different connection intervals and with all or a few sensors enabled.
Part of my issue is that the green LED is not a reliable indicator of power.
Now I turn the SensorTag OFF while watching it on the app.
I am evaluating SensorTag for an application that will require several sensors to be enabled.
Has anyone generated a table that describes the effect on battery performance of each sensor and with different (major) settings?