I'm using the Host Test SPI Example in the CC2650 to control the CC2650 using an external MCU.
Am going to use the defined TI HCI Protocol.
The CC2650 will configured as a peripheral.
Do I need to include the peripheral.c / .h source file to the Host Test Example in order to run the GAP Role peripheral?
Currently my external MCU is able to initialize the GAP profile using the GAP Device Init (0xFE00) and start advertising a profile.