Hi,
My sensor tag is not detecting via the XDS110. Initially I tried flashing the sensor tag code using CCS, and this error showed up.
The XDS110 debug probe is showing in Project->Properties->Connection.
Thinking that this could be a problem with the XDS110 debugger I tried to update the firmware using the xdsdfu tool located in C:\ti\ccsv6\ccs_base\common\uscif\xds110 , and tried running the command using xdsdfu -e, to see the connected XDS110 device,
But the command prompt shows no connected devices, but my device manager shows the connected devices as XDS110 Class Application/User uart COM6 and XDS110 Class Auxillary Data port COM5. It isn't showing up in the Smart RF Flash Programmer 2 too.(The RF Flash and CCS were not open at the same time)
It seems like my XDS110 is bricked, Could anyone from TI help me solve this problem.
Regards,
Shalin