I found that TI CC26xx are one of the lowest power consumption on the market chip sets.
I am looking for audio application.
I found that in the CCS stack everything is configured for the microphone and the speaker and ready to go..
Please for some audio application hints or examples.
I have to connect microphone and speaker via bluetooth at maximum 5 inches distance.
I will have more than 20 sets working simultaneously in the range of 1 feet to 100 yard.
I need to be compatible with some of the popular cellphone bluetooth standards.
I have to provide maximum possible quality, so higher band applications are suitable.
Thank You in advance for the assistance!
eng. Milen Moussakov
milen_01@hotmail.com