Hi there,
I have one of 2650 Sensor Tag board attached to debugger board and trying to run SimpleBLEPeripheral project to see how it works with new TI BLE Stack. I installed the latest CCS 6.1.1.00022 with tirtos_simplelink_setupwin32_2_14_01_20 and xdctools_setupwin32_3_25_06_96. I am using ble_cc26xx_setupwin32_2_01_00_44423 as BLE stack as well.
Unfortunetly I can not compile the SimpleBLEPeripheral project. On Project Properties / CCS General / Main / I set the processor as CC2640F128 and Connections as "Texas Instruments XDDS100v3 USB Debug Probe[Default]". As advance settings Compiler version is TI v5.2.4 and outputformat is eabi (ELF), Device endiannes is little and Linker command file: cc26x0f128.cmd where runtime support library is automatic. On the RTSC tab, I have XDC tools version 3.25.6.96 is selected. I have TI-RTOS for SimpleLink Wireless MCU version 2.14.1.20 and has ${TARGET_CONTENT_BASE} as other repository. On the Order Tab I have ${COM_TI_RTSC_TIRTOSSIMPLELINK_REPOS} first and ${TARGET_CONTENT_BASE} as second. In the end I have Target as ti.targets.arm.elf.M3, Platform as ti.platforms.simplelink:CC2640F128, and Build-profile is set to debug.
However, I am getting following compiler output error as following. I would be very happy if someone can help me on this. Thank you so much!
**** Build of configuration FlashROM for project SimpleBLEPeripheral ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
'Building file: C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Projects/ble/SimpleBLEPeripheral/CC26xx/CCS/Config/appBLE.cfg'
'Invoking: XDCtools'
"C:/ti/xdctools_3_25_06_96/xs" --xdcpath="C:/ti/tirtos_simplelink_2_14_01_20/packages;C:/ti/tirtos_simplelink_2_14_01_20/products/bios_6_42_02_29/packages;C:/ti/tirtos_simplelink_2_14_01_20/products/uia_2_00_02_39/packages;C:/ti/ccsv6/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.M3 -p ti.platforms.simplelink:CC2640F128 -r debug -c "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5" --compileOptions "-mv7M3 --code_state=16 --abi=eabi -me -O4 --opt_for_speed=0 --include_path=\"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/include\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Projects/ble/SimpleBLEPeripheral/CC26xx/Source/Application\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Projects/ble/include\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Projects/ble/ICall/Include\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Projects/ble/Profiles/Roles/CC26xx\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Projects/ble/Profiles/Roles\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Projects/ble/Profiles/DevInfo\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Projects/ble/Profiles/SimpleProfile/CC26xx\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Projects/ble/Profiles/SimpleProfile\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Projects/ble/common/cc26xx\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Components/applib/heap\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Components/ble/hci\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Components/ble/controller/CC26xx/include\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Components/ble/host\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Components/hal/target/CC2650TIRTOS\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Components/hal/target/_common/cc26xx\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Components/hal/include\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Components/osal/include\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Components/services/sdata\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Components/services/saddr\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Components/icall/include\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Components/ble/include\" --include_path=\"C:/ti/tirtos_simplelink_2_13_00_06/products/cc26xxware_2_21_01_15600\" --include_path=\"C:/ti/tirtos_simplelink_2_13_00_06/packages/ti/boards/SRF06EB/CC2650EM_7ID\" -g --gcc --define=USE_ICALL --define=POWER_SAVING --define=SBP_TASK_STACK_SIZE=700 --define=GAPROLE_TASK_STACK_SIZE=520 --define=HEAPMGR_SIZE=2672 --define=TI_DRIVERS_SPI_DMA_INCLUDED --define=TI_DRIVERS_LCD_INCLUDED --define=ICALL_MAX_NUM_TASKS=3 --define=ICALL_MAX_NUM_ENTITIES=6 --define=xdc_runtime_Assert_DISABLE_ALL --define=xdc_runtime_Log_DISABLE_ALL --define=MAX_NUM_BLE_CONNS=1 --define=CC26XXWARE --define=CC26XX --define=ccs --define=DEBUG --diag_wrap=off --diag_suppress=48 --diag_warning=225 --display_error_number --gen_func_subsections=on " "C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Projects/ble/SimpleBLEPeripheral/CC26xx/CCS/Config/appBLE.cfg"
5 [main] sh 14696 tty_list::allocate: No tty allocated
4 [main] sh 13460 tty_list::allocate: No tty allocated
making package.mak (because of package.bld) ...
2 [main] rm 16164 tty_list::allocate: No tty allocated
4 [main] sh 2288 tty_list::allocate: No tty allocated
6 [main] sh 3740 tty_list::allocate: No tty allocated
8 [main] rm 14608 tty_list::allocate: No tty allocated
3 [main] touch 15844 tty_list::allocate: No tty allocated
7 [main] rm 3804 tty_list::allocate: No tty allocated
8 [main] sh 14468 tty_list::allocate: No tty allocated
3 [main] sh 15288 tty_list::allocate: No tty allocated
configuring appBLE.xem3 from package/cfg/appBLE_pem3.cfg ...
5 [main] sh 4772 tty_list::allocate: No tty allocated
js: "C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Projects/ble/SimpleBLEPeripheral/CC26xx/CCS/Config/appBLE.cfg", line 109: XDC runtime error: xdc.runtime.Error: no property named 'policySpin'
"./package/cfg/appBLE_pem3.cfg", line 180
gmake.exe: *** [package/cfg/appBLE_pem3.xdl] Error 1
js: "C:/ti/xdctools_3_25_06_96/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake: *** [configPkg/linker.cmd] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****