Hi,
We are confused by a DCDC problem now. The CC 2640 works in internal DCDC mode. Some chips often work OK for a while after power on (from a few seconds to a few days), then stop working. We check the DCDC_SW pin to find that the voltage drops to about 0.02V (VDDS is OK, 3.2V). After a pin reset (pull Reset pin to ground and release), the chip can be recovered, and the voltage of DCDC_SW pin recovers to 1.6x V.
So what's the possible reason? Thanks a lot !