i want to have a custom advertisement packet, i am using CC2650 simple BLE peripheral example.
The problem is that when i remove flag ad structure and introduce my on ad structure (short name type 0x08) in the packet and compile and run the code, the peripheral device don't connect to android mobile app based central. Altough the peripheral is connectable and its connecting to usb dongle using btool.
Actually i want to create a connectable beacon with custom advertisement packet i dont want to have flag ad structure in the advertisement packet