hi,
i am evaluating the current of RF module.
when i use android phone to pair with devkit by pin code ,the current of RF moduleis up to 13mA,and if there is data transport by SPP link, it is up to 16mA. but if there is no data transport on SPP, the surrent is down to 13mA.and, when android phone disconnected from devkit,the current is down to 3mA.
how can i down the current to 3mA when no data would be transported on SPP?
devkit: MSP-EXP430F5438+MSP5438A+PAN1323+CC256x_MSP430_Bluetopia_SDK_v1-2_Setup.exe
server:devkit
client:android phone(android 2.2)
example:sppdemo
i have checked http://e2e.ti.com/support/low_power_rf/f/660/t/142927.aspx# and http://e2e.ti.com/support/low_power_rf/f/660/p/134853/485099.aspx#485099。but there is not exist code in sppdemo!
best regards
kun