Hi,
I only need to use SPP SPPLE.
How can I optimize SPPLEDemo to get it under 128KB?
What is the stack size? It's larger than 128KB?
When I open SPPLEDemo in iar and go Project->Rebuild all i get
149 726 bytes of CODE memory
7 355 bytes of DATA memory (+ 90 absolute )
38 647 bytes of CONST memory
that is more than 128KB how can run this on MSP430F5529 and MSP430F5229 they only have 128KB of RAM?
Regards,
David.